跳至主要內容
Knowledgebase
Home
Renesas Electronics Taiwan - Knowledgebase

How to select debug tool to use? (CS+)

Last Updated:06/21/2017

Question:

I am using IDE CS+.

How do I select debug tool such as E1 emulator to use?

Answer:

Right-click the debug tool node in the Project Tree panel, and then select the desired tool from the “Using Debug Tool” menu.
See the debug tool edition of each family’s user’s manual to see how to select the debug tool for CS+ for CC.

Note that Simulator is selected when a new project is created on CS+ for CC.

Suitable Products
CS+ (formerly CubeSuite+)