跳至主要內容
Knowledgebase
Home
Renesas Electronics Taiwan - Knowledgebase

How to resolve if I got an error using e CC-RL compiler for RL78 devices?

Latest Updated:07/14/2015

Question:

I am using the CC-RL compiler for RL78 devices. I get the error message below when I designate a library file. How do I resolve this?

E0562201: Illegal library file : "xxxx.lib"

Answer:

Check that you have not designated a library file for CA78K0R. You cannot use the CC-RL compiler to link a library which was generated with CA78K0R because they are in different object formats. Please recreate the library file for CC-RL.
Suitable Products
e² studio
CS+ (formerly CubeSuite+)
C Compiler Package for RL78 Family