跳至主要內容
Knowledgebase
Home
Renesas Electronics Taiwan - Knowledgebase

Downloading by the Evaluation Edition_CS+

Last Updated:12/20/2017

Question:

I am using the evaluation edition of the compiler in the CS+ integrated development environment. Can I perform download to the emulator after the trial period has expired?

Answer:

Yes, you can.

The evaluation edition has the size restriction, but since it only applies to the linkage size, downloading is allowed. The evaluation edition has the following functional restrictions:

    Restriction on the linkage size
    Restriction on the professional edition functions

For details, see the evaluation edition of software tools page.
 

Suitable Products
CS+ (formerly CubeSuite+)
  • 本文是否實用?