跳至主要內容
Knowledgebase
Home
Renesas Electronics Taiwan - Knowledgebase

Can I use the source code generated by the Code Generator tool with an RTOS?

Last Updated:05/17/2017

Question:

Can I use the source code generated by the Code Generator tool with an RTOS?

Answer:

It depends. The Code Generator tool has not been evaluated in use in combination with the RTOS environment. When using the Code Generator tool, combined with the RTOS, you should consider the following conditions in advance and use the code at your own discretion:

1.    The functions and the library generated by the Code Generator tool are not re-entrant.
2.    The Code Generator tool does not take into account interrupt processing in the RTOS.
 

 

Suitable Products
e² studio
CS+ (formerly CubeSuite+)
Code Generator
  • 本文是否實用?