跳至主要內容
Knowledgebase
Home
Renesas Electronics Taiwan - Knowledgebase

Can I use CC-RX V2 & CC-RX V1 for CubeSuite+?

Latest Updated:01/22/2015

Question:

After I updated the version of CubeSuite+, I was no longer able to use the CC-RX compiler.
I have a license for CC-RX V1. Can I use CC-RX V2?

Answer:

CC-RX V1 and CC-RX V2 are separate products which require different license keys.
You need to purchase the following.

Product Name RX Family C/C++ Compiler Package (with IDE) V2
Ordering Number RTCRX0000CL02WDR: Includes a physical medium
RTCRX0000CL02WNR: No physical medium, license only

When you install CubeSuite+ V2, the free evaluation version of CC-RX V2 is also installed.
In this case, you will still be able to use the product version of CC-RX V1 by changing the version number of the compiler to be used.
For how to change the version number of the compiler, refer to FAQ1011387.

Suitable Products
CS+ (formerly CubeSuite+)
C/C++ Compiler Package for RX Family