跳至主要內容
Knowledgebase
Home
Renesas Electronics Taiwan - Knowledgebase

CS+ on the Windows task bar (CS+ Integrated Development Environment)

Last Updated:06/072017

Question:

I am using the CS+ integrated development environment.

The CS+ icon is displayed in the system tray (notification area) on the Windows task bar.

Why does this icon appear?

Answer:

Because the rapid start function of CS+ is enabled, the CS+ icon is displayed in the system tray (notification area).

The rapid start function makes CS+ permanently resident to accelerate the startup time. This function is enabled by default.

To enable or disable the rapid start, select the [General - Startup and Exit] category in the Option dialog box, and then select or clear the [Reduce startup time by enabling rapid startup] check box.

For details about the [General - Startup and Exit] category in the Option dialog box, see this site.

Suitable Products
CS+ (formerly CubeSuite+)
  • 本文是否實用?