跳至主要內容
Knowledgebase
Home
Renesas Electronics Taiwan - Knowledgebase

Why is it impossible to terminate High performance Embedded Workshop?

Latest Updated:10/23/2013

Question:

When I use the command line function of High-performance Embedded Workshop to automatically run a series of operations from saving sessions from a batch file (SAVE_SESSION) to terminating High-performance Embedded Workshop (QUIT), a message prompting for confirmation of whether or not to save is displayed again for the sessions that must have been saved when High-performance Embedded Workshop is closed, making it impossible to automatically terminate.

Answer:

Execute the commands CLOSE_WORKSPACE and QUIT in that order without using the SAVE_SESSION command.
However, if you want to save window position information in a session file, run “Save Session" from the menu before executing a batch file.

* The SAVE_SESSION command does not save window position information in a session file.

Suitable Products
High-performance Embedded Workshop