跳至主要內容
Knowledgebase
Home
Renesas Electronics Taiwan - Knowledgebase

Why building operation did not stop even if I click execute Build in menu

Latest Updated:09/10/2007

Question:

[High-performance Embedded Workshop V.4, V.3]  Even though I clicked an execute Build from the Build menu,the building operation did not stop. Why?

Answer:

Execute Build is canceled after executing the Build command for the current file(or executing the current phase) in High-performance Embedded Workshop.

Please choose [Build->Terminate Current Tool] If you don't recieve a reply after awhile from project builder, the current process may have crashed. A file which is output from a crashed tool is invalid.

Please re-execute the phase by deleting these output files.

Suitable Products
High-performance Embedded Workshop