跳至主要內容
Knowledgebase
Home
Renesas Electronics Taiwan - Knowledgebase

How to use STKViewer and MAPViewer from an M32R, M32C or M16C project?

Latest Updated:09/10/2007

Question:

[High-performance Embedded Workshop4, 3 specific]  How can I use STKViewer and MAPViewer from an M32R, M32C or M16C project?

Answer:

Please set up High-performance Embedded Workshop in the following procedure.
  1. In the menu, click [Tools] -> [Customize] to display the Customize dialog box.
  2. Click the Menu tab in the Customize dialog box.
  3. Click the Add button to display the Add Tool dialog.
  4. Specify the following in the Add Tool dialog.
  • To use STKViewer (example)
    Name STKViewer
    (any name is acceptable)
    Command C:\MTOOL\BIN\stkviewer\jre\1.2\bin\javaw.exe
    (specify the javaw.exe in the compiler install directory)
    Arguments -Xmx600m -jar C:\MTOOL\BIN\StkViewer.jar -x $(CONFIGDIR)$(PROJECTNAME).x30
    (specify the stkviewer.jar in the compiler install directory)
    Initial directory $(CONFIGDIR)

     
  • To use MAPViewer (example)
    Name MAPViewer
    (any name is acceptable)
    Command C:\MTOOL\BIN\MapViewer.exe
    (specify the mapviewer.exe in the compiler install directory)
    Arguments $(CONFIGDIR)$(PROJECTNAME).x30
    Initial directory $(CONFIGDIR)
Suitable Products
High-performance Embedded Workshop