跳至主要內容
Knowledgebase
Home
Renesas Electronics Taiwan - Knowledgebase

How can I set a cycle number when accessing to an external memory space?

Latest Updated:09/10/2007

Question:

How can I set a cycle number when accessing to an external memory space?

Answer:

Choose Option from High-performance Embedded Workshop menu, then choose simulator, then Memory Source. A dialog box for memory settings for simulator will open. Please double-click at a memory space on memory map which you want to set an access cycle, and set it. Moreover, if you simulator supports Bus State Controller (BSC), you can reflect the setting to the memory map by setting a register for BSC in your program.
Suitable Products
High-performance Embedded Workshop
C/C++ Compiler Package for SuperH Family
C/C++ Compiler Package for H8SX, H8S, H8 Family