跳至主要內容
Knowledgebase
Home
Renesas Electronics Taiwan - Knowledgebase

Can I use the work space in old High-performance Embedded Workshop3?

Latest Updated:09/10/2007

Question:

I updated High-performance Embedded Workshop3 to High-performance Embedded Workshop4.
When I opened a workspace generated in High-performance Embedded Workshop3 while in High-performance Embedded Workshop4, the workspace files were automatically revised.
Can I use the workspace in the old High-performance Embedded Workshop3 environment?

Answer:

Yes, you can still use the workspace in the High-performance Embedded Workshop3 environment using the following procedures.

  1. Make a backup (copy) of the workspace folder.
  2. You will find several backup files that have the string "old_version_xxx" in their names in the workspace folder.
    Confirm the backup files and the revised files.
  3. Delete the revised files (file names that do not include “old_version_xxx”)
  4. Rename the backup files (remove "old_version_xxx" from the backup file names). Several backup files must be renamed at the same time.
  5. Uninstall the High-performance Embedded Workshop4 environment.
  6. After re-installing the High-performance Embedded Workshop3 environment, open the workspace.

Note 1:
Project operations (add files to project, change build options, etc.) done in the High-performance Embedded Workshop4 environment are invalid.
Note 2:
Workspaces cannot be opened in High-performance Embedded Workshop environments older than the one in which they were originally created.

Suitable Products
High-performance Embedded Workshop