跳至主要內容
Knowledgebase
Home
Renesas Electronics Taiwan - Knowledgebase

Does FDT need an adapter board for SuperH, H8SX, H8S or H8 Family MCUs?

Latest Updated:05/14/2009

Question:

[Flash Development Toolkit V.2, V.3, V.4] Does the FDT need an adapter board for the development of SuperH, H8SX, H8S or H8 Family MCUs?

Answer:

Adapter board is not necessarily.
It is hardware which generates reset signal and sets mode pins.
It also shifts voltage levels of serial communication signals.
You do not have to use an adapter board if you have the same functional interface circuitry on the target board.
Suitable Products
Flash Development Toolkit