跳至主要內容
Knowledgebase
Home
Renesas Electronics Taiwan - Knowledgebase

Can each emulator be used through FDTK when connecting emulator to 1 PC?

Latest Updated:04/11/2012

Question:

[Flash Development Tool Kit V.4] When connecting several on-chip debugging emulators to one PC, can I use each emulator through the Flash Development Tool Kit?

Answer:

Yes, you can if you are using E1, E20 or E8a.
Each emulator has a unique serial number, which enables the Flash Development Tool Kit to recognize multiple emulators. Therefore, you can start up several Flash Development Tool Kits and write to several target MCUs from a single PC.
However, you cannot operate multiple emulators from the window of just one Flash Development Tool Kit.

flash_106942_en_1.gif

 

Suitable Products
Flash Development Toolkit