跳至主要內容
Knowledgebase
Home
Renesas Electronics Taiwan - Knowledgebase

What is the zero-cross frequency of an operational amplifier?

Latest Updated:12/01/2011

Question:

What is the zero-cross frequency of an operational amplifier?

Answer:

The zero-cross frequency is the frequency at which the open loop voltage gain becomes 0 dB (×1) and is calculated from the Aυ vs. f characteristics.
Suitable Products
Operational Amplifiers
USB2.0 Host/Peripheral Controller
UPD720150