跳至主要內容
Knowledgebase
Home
Renesas Electronics Taiwan - Knowledgebase

What is the capacitance between pins in an RD series diode?

Latest Updated:09/01/2006

Question:

What is the capacitance between pins in an RD series diode?

Answer:

The RD series has been developed for reference voltage, voltage detection, level shift and other such applications, so the capacitance between pins is not prescribed.
We advise you to use a product with a prescribed pin-to-pin capacitance, such as the NNCD series or NSAD series, which has been developed for high-speed signal line ESD protection and surge absorption applications.
Suitable Products