跳至主要內容
Knowledgebase
Home
Renesas Electronics Taiwan - Knowledgebase

What is the channel to ambient thermal resistance (θch-a) of 2SK3157?

Latest Updated:09/02/2013

Question:

I would like to use a MOSFET (2SK3157) without a heat sink. What is the channel to ambient thermal resistance (θch-a)?

Answer:

The reference value for channel to ambient thermal resistance (θch-a) of the 2SK3157 is 50 ℃/W measured from an arbitrary sample.

*This data is not a guaranteed value.

Suitable Products
Power MOSFETs for General Switching