How much is the reverse recovery time (trr) of the RJK60S5DPK-M0?
Latest Updated:09/02/2013
Question:
How much is the reverse recovery time (trr) of the RJK60S5DPK-M0?
Answer:
Reverse recovery time trr is specified as "Body-drain diode reverse recovery time [trr]" in the datasheet, which is 400 ns Typ.
This article is written based on not recommended products.
Suitable Products
Power MOSFETs for General Switching |