跳至主要內容
Knowledgebase
Home
Renesas Electronics Taiwan - Knowledgebase

Can I use the UPD5200, 5201, or 5205 with a single power supply?

Latest Updated:09/01/2007

Question:

Can I use the UPD5200, 5201, or 5205 with a single power supply?

Answer:

Each of uPD5200, uPD5201, and uPD5205 is specified for use with a dual power supply, so you must not use it with a single power supply. Use it under the recommended conditions listed in the Data Sheet.
Suitable Products