跳至主要內容
Knowledgebase
Home
Renesas Electronics Taiwan - Knowledgebase

What are the output characteristics of the uPC803?

Latest Updated:12/01/2011

Question:

What are the output characteristics of the uPC803?

Answer:


Data of the uPC803 at hand were measured. The results are as shown on the left.
Use this data for your reference.

Test conditions: Room temperature (approx. 25°C)
Supply voltage: ±15 V

Note that this data is a product that happened to be at hand and that the results are not guarantee values.

 
 
 
Suitable Products