跳至主要內容
Knowledgebase
Home
Renesas Electronics Taiwan - Knowledgebase

Is it okay the Tj is 0 to 125°C if the temperature condition is not shown?

Latest Updated:12/01/2011

Question:

There are three parameters of VO for the uPC7805A.
The temperature conditions of two are shown but those of the third are not.
Is it all right to consider that Tj of the parameter whose temperature conditions are not shown is 0 to 125°C?

Answer:

That is correct; Tj is 0 to 125°C.
The conditions (common conditions) shown in the margin are applied to a parameter whose conditions are not shown.
These conditions are also applied to the parameter in question.
Suitable Products
CMOS Operational Amplifiers
Bipolar Operational Amplifiers
3 Terminal Regulators