跳至主要內容
Knowledgebase
Home
Renesas Electronics Taiwan - Knowledgebase

What is the thermal resistance of 2SK1292 (discontinued product)?

Latest Updated:09/02/2013

Question:

How much is the thermal resistance of the 2SK1292 (discontinued product)? It's not in the datasheet.

Answer:

The thermal resistance of the 2SK1292 is as follows.

  • Channel to case thermal resistance = 3.57 ℃/W
  • Channel to air thermal resistance = 62.5 ℃/W
Suitable Products
Power MOSFETs for General Switching