跳至主要內容
Knowledgebase
Home
Renesas Electronics Taiwan - Knowledgebase

Are there any product that can pass the range of supply voltage?

Latest Updated:12/01/2011

Question:

Are there rail-to-rail operational amplifiers whose input and output voltages can be up to the range of the supply voltage?

Answer:

Unfortunately we do not provide rail-to-rail operational amplifiers.
However, we are developing the product now.
Suitable Products
Operational Amplifiers
USB2.0 Host/Peripheral Controller
M66596, R8A66597
UPD720150