跳至主要內容
Knowledgebase
Home
Renesas Electronics Taiwan - Knowledgebase

What is a series regulator with 2 output functions?

Latest Updated:10/01/2006

Question:

What is a series regulator with 2 output functions?

Answer:

This is a series regulator that outputs two different output voltages from an input voltage (in single package).

Example: The UPC37Mxx Series consists of regulators that have two output functions, OUTPUT1 (3.3 V or 2.5 V): 1 A and OUTPUT2 (1.8 V or 2.5 V): 0.5 A.

Suitable Products
Power Management Linear
  • 本文是否實用?