跳至主要內容
Knowledgebase
Home
Renesas Electronics Taiwan - Knowledgebase

What is output applied voltage of an operational amplifier?

Latest Updated:12/01/2011

Question:

What is output applied voltage of an operational amplifier?

Answer:

This is the range of voltage that can be applied to the output pins without degrading the characteristics or damaging the device.
This rating must never be exceeded, even in the transient state when the power is being turned on and off
Note that the output voltage obtained via an operational amplifier must not exceed the maximum output voltage prescribed in the electrical specifications of the device.
Suitable Products
Operational Amplifiers
UPD720201
UPD720100A