跳至主要內容
Knowledgebase
Home
Renesas Electronics Taiwan - Knowledgebase

What are the temperature characteristics of the VBE?

Latest Updated:03/01/2006

Question:

Data of the VBE at low temperatures and at high temperatures are not shown in the Data Sheet. What are the temperature characteristics of the VBE?

Answer:

The temperature characteristics of the VBE are determined by the temperature coefficient of the PN junction (-2 mV/°C).
Suitable Products