跳至主要內容
Knowledgebase
Home
Renesas Electronics Taiwan - Knowledgebase

TPS-1 WD_OUT Output Control

Last Updated:06/01/2017

Question:

Can the customer control the output of WD_OUT on the TPS-1?

Answer:

The WD_OUT output is driven automatically by the TPS-1, however, the reaction to WD_OUT by the host CPU can be changed by the customer.
Suitable Products
TPS-1
  • 本文是否實用?