跳至主要內容
Knowledgebase
Home
Renesas Electronics Taiwan - Knowledgebase

TPS-1 External 1.5V Regulator

Last Updated:06/01/2017

Question:

Can an external 1.5V regulator be used instead of the TPS-1 internal 1.5V regulator?

Answer:

Yes, an external 1.5V can be used for TPS-1. When using an external 1.5V regulator, please pull up TEST1 pin to change the 1.5V internal regulator output (Pin LX) to hi-Z status.
Suitable Products
TPS-1
  • 本文是否實用?