Is the bit count be an integral multiple of the 10-bits sign pair length?
Latest Updated:08/01/2005
Question:
For the uPD98408 ATM PHY, is the interval (bit count) between adjacent pairs of signs separated by the IDLE pattern in the PHY output direction so as to be an integral multiple of the sign pair length (10 bits)?
Answer:
Yes, that is correct.
Suitable Products
BD/DVD Recorder |
Digital Camcorder |
Industrial Network |