跳至主要內容
Knowledgebase
Home
Renesas Electronics Taiwan - Knowledgebase

sf_touch_panel_i2c Module Guide Resources

Last Updated:10/09/2017

Question:

Where can I find the references to module guide resources for the Module module on module?

Answer:

Introduction

The Touch Panel I2C Framework module provides a high-level API for reading messages from a touch controller and is implemented using an I2C port. The Touch Panel Framework module uses the IIC or SCI peripherals on the Synergy MCU.

The Touch Panel I2C Framework module supports the following features:

  • Reads data from a touch controller and publishes touch messages to any queue subscribed to touch events in the messaging framework
  • Provides position data (X and Y coordinates)
  • Provides the touch event type (down, up, move, hold, or invalid)
  • Supports I2C-based touch panel implementations with external interrupts

Module Guide

The Touch Panel I2C Framework module guide is targeted for SSP 1.2.0 (and above) and the SK-S7G2 Kit.

The most recent versions of the Touch Panel I2C Framework module guide application note, application project and import guide are available here.

Known issues

  • Refer to the SSP release notes for known issues, available here.
Suitable Products
SSP 1.2.0 and above
  • 本文是否實用?