跳至主要內容
Knowledgebase
Home
Renesas Electronics Taiwan - Knowledgebase

sf_power_profiles_v2 Module Guide Resources

"Last Updated" copy

Question:

Where can I find the module guide resources for the Power profiles V2 framework module on sf_power_profiles_v2?

Answer:

Information on the module guide itself and the associated resources and known issues are available here.

Introduction

The Power Profiles V2 (PPv2) Framework provides more control for users to set a power control mode and the LPM mode in the Synergy MCU. The PPv2 Framework supports all the features of the Power Profiles v1 available in the current release of the Synergy Software Program (SSP) Framework using the LPM v1 driver. The Power Profiles v1 and PPv2 Framework are not compatible. Power Profiles v1 and PPv2 Framework cannot be used in the same project. For all new projects, it is recommended that applications use PPv2 Framework.

The Power Profiles V2 Framework has the following features:

  • Configurable options to set different MCU power control modes with customizable clock domains.
  • Configurable options to set different MCU low power modes with different IO port or pin configurations.
  • Supports both threaded and non-threaded operations

Module Guide

The Power Profiles V2 Framework module guide is targeted for SSP 1.2.0 and above and the SK-S7G2 Kit.

The Power Profiles V2 Framework module guide application note, application project and import guide are not yet available.

Module Guide Resources

  • Content provided as it becomes available.

Known issues

  • Refer to the SSP release notes for known issues, available here.
SSP
  • 本文是否實用?