跳至主要內容
Knowledgebase
Home
Renesas Electronics Taiwan - Knowledgebase

r_rtc Module Guide Resources

Last Updated:11/27/2017

Question:

Where can I find the references to module guide resources for the RTC HAL module on r_rtc?

Answer:

Information on the module guide itself and the associated resources and known issues are available here.

Introduction

The Real-Time Clock (RTC) HAL module is a high-level API for RTC applications and is implemented on r_rtc. The RTC HAL module configures the RTC module and controls clock, calendar, and alarm functions. The RTC uses the real-time clock module on the Synergy MCU. A user-defined callback can be created to respond to any of the three supported interrupt types- alarm, periodic, or carry.

The RTC HAL module supports the following features:

  • RTC peripheral configuration
  • Clock and calendar functions:
  • Alarm, periodic, and carry interrupts
  • Time-capture function
  • Event linkage to other peripherals

Module Guide

The r_rtc HAL module guide is targeted for SSP 1.2.0 and above and the SK-S7G2 Kit.

The most recent versions of the RTC HAL module guide application note, application project and import guide are available here

Module Guide Resources

  • The RTC HAL module is used in the Developer Examples available for the DK-S7G2. You can find a Knowledge Base article that describes the Developer Examples and how to create a project using the template here.

Known issues

  • Refer to the SSP release notes for known issues, available here.
Suitable Products
SSP
  • 本文是否實用?