跳至主要內容
Knowledgebase
Home
Renesas Electronics Taiwan - Knowledgebase

r_opamp Module Guide Resources

Last Updated:02/27/2018

Question:

Where can I find the references to module guide resources for the Operational Amplifier HAL module on r_opamp?

Answer:

Information on the module guide itself and the associated resources and known issues are available here.

Introduction

The Operational Amplifier HAL module implements high-level APIs for signal amplification applications on r_opamp. It supports the OPAMP peripheral available on Synergy MCUs.

This module supports the following features:

  • Low power or high-speed mode
  • Start by software or AGT compare match
  • Stop by software or ADC conversion end (stop by ADC conversion end only supported on op-amp channels configured to start by AGT compare match)
  • Trimming available on some MCUs (see hardware manual)

 

Module Guide

The module guide is not yet available.

 

Module Guide Resources

There are currently no resources available for this module.

 

Known issues

  • Refer to the most current SSP release notes for any known issues.
Suitable Products
SSP
  • 本文是否實用?