跳至主要內容
Knowledgebase
Home
Renesas Electronics Taiwan - Knowledgebase

r_icu Module Guide Resources

Last Updated:11/22/2017

Question:

Where can I find the references to module guide resources for the External Interrupt Controller module on r_icu?

Answer:

Information on the module guide itself and the associated resources and known issues are available here.

Introduction

The External IRQ HAL module is an API for External IRQ applications and is implemented on r_icu. The External IRQ HAL module uses the Interrupt Controller Unit (ICU) on the Synergy MCU. A user-callback function can be used and can be triggered each time an IRQ event occurs.

The External IRQ HAL module supports the following features:

  • Supports the External interrupt pins available on the target Synergy MCU
  • Supports multiple function options

Module Guide

The External Interrupt HAL module guide is targeted for SSP 1.2.0 and above and the SK-S7G2 Kit.

The most recent versions of the External Interrupt HAL module guide application note, application project and import guide are available here

Module Guide Resources

The following application projects are available from the Renesas web site at the referenced url.

  • Bluetooth Low Energy on DK-S7G2 and DK-S3A7 - Application Project here
  • Getting Started with the Weather Panel Application - Application Project here
  • The External IRQ HAL module is used in the Developer Examples available for the DK-S7G2. You can find a Knowledge Base article that describes the Developer Examples and how to use them here.

Known issues

  • Refer to the most current SSP release notes for any known issues.
Suitable Products
SSP
  • 本文是否實用?