跳至主要內容
Knowledgebase
Home
Renesas Electronics Taiwan - Knowledgebase

Why do I get a configuration issue when I use the Threaded Blinky Template?

Latest Updated:10/13/2016

Question:

Why do I get a configuration issue when I load up the Threaded Blinky template?

Answer:

The configuration file for Threaded Blinky is missing a check box for RTOS inclusion. Just add that in under the BSP tab as instructed by the error indicator. This has been fixed in the SSP 1.1.0 and beyond releases.

 

  • 本文是否實用?