Where do I find updates to the DK-S3A7 Kit information and examples?
Latest Updated:10/13/2016
Question:
Where do I find updates to the DK-S3A7 kit information, examples and issues?
Answer:
You can find all the updates to the DK-S3A7 kit information, examples and issues here.
1) What are the specifications for the LCD panel used on the DK-S3A7 V2 Kit?
You can find a Knowledge base article with the information here:
What are the specifications for the DK-S3A7 V2 LCD Panel?
2) What are the correct switch settings to enable JTAG on the DK-S3A7 V2 kit?
What are the JTAG switch settings for Synergy kits to enable debugging?