跳至主要內容
Knowledgebase
Home
Renesas Electronics Taiwan - Knowledgebase

How do you get the Synergy custom BSP creator to work? Im having problems with the app note

Latest Updated:10/13/2016

Question:

I'm having a problem creating a Custom BSP using the app note on the Synergy Gallery. What do I need to do?

https://synergygallery.renesas.com/media/products/22/38/en-US/r01an3044eu0102_synergy.pdf

Answer:

There is a missing step in the app note that needs to be added. The change is shown below:

The workaround is to add a step after step 1 in Section 2.3:

 

[Existing Step 1] After the project has been created, e2 studio must be configured to treat the BSP module as a template module. Only perform this step when working with template pack BSPs.

 

New #2. Select the Components pane. In the list, check the box next to Common >> all >> ssp_common. Save your project.

[Existing Step 2, New Step 3] 2. Close e2 studio.