跳至主要內容
Knowledgebase
Home
Renesas Electronics Taiwan - Knowledgebase

What do I do to create a C++ project in Synergy using SSP 1.3.0 and later?

"Last Updated" copy

Question:

What do I need to do to create a C++ project using SSP 1.3.0 and later?

Answer:

Creating a C++ project is easy in SSP 1.3.0 and later. Just select File, New and Project as shown below.
CplusPlus.png
This will bring up the project wizard shown below. Select Synergy C++ Project and click next.
CplusPlusProject.png
The wizard will build a C++ project for you and you populate it the same way as a normal project.
 
SSP 1.3.0 and later
  • 本文是否實用?