跳至主要內容
Knowledgebase
Home
Renesas Electronics Taiwan - Knowledgebase

What Performance can I expect with Ethernet, SSP and NetX?

Last Updated: 04/08/2016

Question:

What Ethernet performance can I expect to see when using NetX and SSP?

 

Answer:

There are benchmark results listed in the SSP data sheet.

TCP Receive 83 Mbps

TCP Transmit 28 Mbps

UDP Receive 91 Mbps

UDP Transmit 94 Mbps

The SSP data Sheet is available here:

https://www.renesas.com/en-us/products/synergy/software.html# 

  • 本文是否實用?