跳至主要內容
Knowledgebase
Home
Renesas Electronics Taiwan - Knowledgebase

What is the peripheral I/O board IE-703102-MC-EM1-A used for?

Latest Updated:12/01/2011

Question:

What is the peripheral I/O board IE-703102-MC-EM1-A used for?

Answer:

The IE-703102-MC-EM1-A board is used in combination with the IE-703102-MC to emulate the functions of peripheral I/O in products such as the uPD703102A.
That is, by combining IE-703102-MC (which emulates the CPU core part) and this board IE-703102-MC-EM1-A, total device emulation is enabled.
Suitable Products
V850 Family