跳至主要內容
Knowledgebase
Home
Renesas Electronics Taiwan - Knowledgebase

Where does code coverage display the information on C1 coverage?

Latest Updated:01/05/2016

Question:

When I use a simulator debugger for a SuperH device to measure code coverage, where does it display the information on C1 coverage?

Answer:

The C1 coverage is displayed in [Coverage-ASM] if the source file is being displayed in a disassembly mode or a mixed mode in the editor window of HEW. The information displayed is as follows.

  • T: The condition of the conditional branch instruction is always satisfied.
  • F: The condition of the conditional branch instruction is never satisfied.
  • T/F: The condition of the conditional branch instruction sometimes is and sometimes is not satisfied.
Suitable Products
Simulator Debugger for SuperH Family [for High-performance Embedded Workshop]