跳至主要內容
Knowledgebase
Home
Renesas Electronics Taiwan - Knowledgebase

What happen to section: L1120 address not assigned to section name

Latest Updated:09/10/2007

Question:

I got an error message "L1120(W) Section address is not assigned to section name". 
What happens to the appropriate section ?

Answer:

The appropriate section is assigned to right after the section with the biggest address of all the sections that are assigned to the optimizing linkage editor.
Suitable Products
C/C++ Compiler Package for SuperH Family
C/C++ Compiler Package for H8SX, H8S, H8 Family