跳至主要內容
Knowledgebase
Home
Renesas Electronics Taiwan - Knowledgebase

What do block numbers become in boot swapping on FSPL Type01 for RL78?

Latest Updated:10/24/2014

Question:

If I am specifying block numbers for functions, what do the block numbers become after boot swapping by Flash Self Programming Library Type01 for the RL78 family ?
For example, if I am specifying the blocks for addresses 01000H to 01400H in the RL78/G13, are block numbers 00H and 04H swapped each time boot swapping proceeds ?

Answer:

You do not need to swap block numbers before and after boot swapping. You can specify the block numbers corresponding to addresses in the user area.
For the RL78/G13, the block number for addresses 01000H to 01400H is always 04H.
Suitable Products
Flash Self Programming Libraries