跳至主要內容
Knowledgebase
Home
Renesas Electronics Taiwan - Knowledgebase

What's the meaning of ".POOL" and ".NOPOOL" assembler source program?

Latest Updated:12/01/2009

Question:

What's the meaning of ".POOL" and ".NOPOOL" assembler source program?

Answer:

These are assembler directives which can control the behavior of the assembler.

".POOL" specify an output position of the literal pool in case of using the Automatic Literal Pool Generation Function. ".NOPOOL" to output the literal pool in case of using the Automatic Literal Pool Generation Function.

Suitable Products
C/C++ Compiler Package for SuperH Family