跳至主要內容
Knowledgebase
Home
Renesas Electronics Taiwan - Knowledgebase

What's the meaning of "-ws" option in "LNK -ws=.$OPT0000.SUB" ?

Latest Updated:09/10/2007

Question:

"LNK -ws=.$OPT0000.SUB" is described in the makefile. What's the meaning of "-ws" option?

Answer:

This is a sub command file specification option used internally between the HEW and the compiler.

This option is not written in the manual.

Suitable Products
C/C++ Compiler Package for SuperH Family
C/C++ Compiler Package for H8SX, H8S, H8 Family