跳至主要內容
Knowledgebase
Home
Renesas Electronics Taiwan - Knowledgebase

PDG Ver2 Multiple Interrupts Support

Last Updated:08/24/2017

Question:

Does PDG (Ver. 2) support multiple interrupts? Or, is it intended to incorporate this capability in the future?

Answer:

PDG (Ver. 2) does not support multiple interrupts.
Development of PDG was terminated in 2013. Therefore, PDG will not support this capability.
However, you can achieve multiple interrupts by using an interrupt function declared by #pragma interrupt to enable multiple interrupts. For details, see the following manual.

CC-RX Compiler User's Manual
4. COMPILER LANGUAGE SPECIFICATIONS
4.2 Extended Language Specifications
4.2.4 Using Extended Specifications
(3) Interrupt Function Creation

Suitable Products

C/C++ Compiler Package for RX Family
Peripheral Driver Generator