跳至主要內容
Knowledgebase
Home
Renesas Electronics Taiwan - Knowledgebase

Is size of library fixed in user's manual of RL78 FDFL Type04 ?

Latest Updated:04/04/2014

Question:

Is the size of the library described in user’s manual of RL78 Family Data Flash Library Type04 fixed?

Answer:

No, it isn’t.
The size described in the manual is for the case when all functions including the PFDL_GetVersionString function (the function for acquiring the version information of Data Flash Library Type04) are in use.
Not using the PFDL_GetVersionString function of Data Flash Library Type04 V1.05 can reduce the size by 25 bytes.
Suitable Products
Data Flash Libraries