跳至主要內容
Knowledgebase
Home
Renesas Electronics Taiwan - Knowledgebase

How to make software without interrupting handler auto function?

Latest Updated:12/01/2011

Question:

I want to build software (including a RESET interrupt), without using the interrupt handler automatic allocation function (#pragma Interrupt interrupt-request-name function-name).
How can I build such software?

Answer:

When you use C language, there is no other description method except using the interrupt handler automatic allocation function.
If you have to use another method, describe in assembly language.
Refer to the interrupt example in the Q&A (Q.1.14) of the Tutorial Guide.

V800 Series (TM) Development Tool Tutorial Guide Windows (TM) Based
Suitable Products