跳至主要內容
Knowledgebase
Home
Renesas Electronics Taiwan - Knowledgebase

How to deal with this error message "Invalid Load Address"?

Latest Updated:09/15/2006

Question:

I am getting the error message "Invalid Load Address". How should I deal with it?

Answer:

When extracting data from a mask file, you cannot extract hexadecimal data in an Intel HEX format under the following conditions.
1. When an S3 format record is included in the mask file.
2. When the address you are using in your program exceeds the 20-bit limit.
In these conditions, data must be extracted in the Motorola S format.
Please refer to Appendices A and B of the MM User's Manual for details concerning file formats.
Suitable Products
Maskfile Converter
4500 Series ROM Ordering
720 Series ROM Ordering
38000 Series ROM Ordering
740/7450/7470 Series ROM Ordering
7600 Series ROM Ordering
7200 Series ROM Ordering
7770 Series ROM Ordering
M16C Family ROM Ordering
R8C Family ROM Programmed Shipment Ordering
QzROM Programmed Shipment Ordering
ASSP ROM Ordering
OSD Controller ROM Ordering