跳至主要內容
Knowledgebase
Home
Renesas Electronics Taiwan - Knowledgebase

How to deal with this error message "Can't open file filename"?

Latest Updated:09/15/2006

Question:

I am getting the error message "Can't open file filename". How should I deal with it?

Answer:

This message means that the file specified as filename could not be opened. Please check the actual file name again and set the name to an existing file.
This error message is also displayed when a mask file is created with MM V.3.00 Release 1 and the following 2 conditions are met.
1. MM is executed on Windows Me/98/95.
2. The hexadecimal data file to be processed is located in a root directory such as C:¥.
When using MM in Windows Me/98/95, locate the hexadecimal data file in a directory other than the root directory.
Suitable Products
Maskfile Converter
4500 Series ROM Ordering
720 Series ROM Ordering
38000 Series ROM Ordering
740/7450/7470 Series ROM Ordering
7600 Series ROM Ordering
7200 Series ROM Ordering
7770 Series ROM Ordering
M16C Family ROM Ordering
R8C Family ROM Programmed Shipment Ordering
QzROM Programmed Shipment Ordering
ASSP ROM Ordering
OSD Controller ROM Ordering