跳至主要內容
Knowledgebase
Home
Renesas Electronics Taiwan - Knowledgebase

How should ROM Programming Confirmation Form be filled out?

Latest Updated:09/15/2006

Question:

[R8C/Tiny] How should ROM Programming Confirmation Form be filled out?

Answer:

Please refer to the following examples.

Suitable Products
Maskfile Converter
4500 Series ROM Ordering
720 Series ROM Ordering
38000 Series ROM Ordering
740/7450/7470 Series ROM Ordering
7600 Series ROM Ordering
7200 Series ROM Ordering
7770 Series ROM Ordering
M16C Family ROM Ordering
R8C Family ROM Programmed Shipment Ordering
QzROM Programmed Shipment Ordering
ASSP ROM Ordering
OSD Controller ROM Ordering